Wifi6 - Wait and See or Act Today
Available On Demand
Summary
Wifi6 or 802.11ax is available for large scale commercial and is driven by benefits like 4X higher capacity, increased security and reduced latency. For the first time, multiple Wi-Fi clients can transmit or receive concurrently using orthogonal frequency-division multiple access (OFDMA) with allocated resource units. The challenge increases dramatically as the number of simultaneous users scale up in a diverse client mix at varying distances.
Traditional test tools that are based on commercial chipsets or using real-client devices cannot address these challenges. A next-generation test tool capable of simulating multi-user OFDMA at scale is required to fully validate the functionality and performance gain promised by 802.11ax technology.
Keshav Sudial
Pre-Sales Application Engineer,
Network Solutions and Sales
Keysight Technologies
Keshav takes care of pre-sales activities for the Wi-Fi product line for Keysight India. He mainly works with AP manufacturers, chip vendors and companies who work in Wi-Fi technology. He helps customers in resolving their queries around this new technology and helps them in implementing solutions involving Keysight's Wi-Fi products. He also looks after the 5G Core and IxChariot business for Keysight India.